.NET Framework Version 1.1 Full Install
This software package comprises the material to install Microsoft .NET framework 1.1. The user expressly acknowledges and agrees that he is installing and using the provided material at his own sole risk. We provide no remedies or warranties, whether express or implied, for the material. It is provided “as is” without warranty, term or condition of any kind. Information on the different material can be received through www.microsoft.com.
Material 1: .NET Framework Version 1.1 'dotnetfx.exe'
Material 2: .NET Framework Version 1.1 Service Pack 1 (KB867460) 'NDP1.1sp1-KB867460-X86.exe'
Material 3: .NET Framework 1.1 post-Service Pack 1 hotfix rollup package (KB887540) 'NDP1.1sp1-KB887540-X86.exe'
Installation process
- Click the download link ".NET Framework 1.1 Full Install" on www.pepperl-fuchs.com to start the download
- Unzip the downloaded ZIP file to a folder of your choice
- Run the "setup.exe" program in this folder and wait for the SETUP start screen
- Click on each of the 3 installation packages in the window to the left to highlight them all
- Click to the Button "Install selected applications" to start the installation procedure
- Follow all 3 installation instructions on the screen and if necessary confirm the asked questions
- Wait for all 3 packages to complete the installation
- .NET framework 1.1 + Service Pack 1 + hotfix rollup package installation is now completed
|