PACTware 3.6 SP1
PACTware Consortium e.V.

Copyright (C) 1999-2009 PACTware Consortium e.V.
All rights reserved
===============================================================================
Contents
===============================================================================
 1. Overview
 2. Software requirements
 3. Hardware requirements
 4. Installation
 5. Deinstallation
 6. Start PACTware
 7. Known Problems
 8. Changes in this version
 9. Error messages
10. Download .NET Framework 1.1 and .NET Framework 1.1 SP 1

===============================================================================
1. Overview
===============================================================================
 PACTware (Process Automation Configuration Tool) is a program designed to combine
 communication-capable field devices of different vendors in projects.
 PACTware is used in accordance with the FDT Specification 1.2.1 (Field Device Tool Specification) 
 as frame program for DTMs (Device Type Manager), which are provided as configuration software 
 by field device vendors. The communication with field devices using protocols like
 e.g. the HART or Profibus protocol is established via a CommDTM (Communication DTM).
  
===============================================================================
2. Software requirements
===============================================================================
 PACTware runs under the operating system Windows 2000 SP4, Windows XP, 
 Windows XP SP1 to SP3 and Windows Vista. 
 To use the print functions and Online Help MS Internet Explorer 4.0 or higher is required.
 
 Windows 95, 98, ME and NT 4.0 are not supported by this PACTware release.

===============================================================================
3. Hardware requirements
===============================================================================
 PACTware requires 100 MByte disk space, 50 MByte main memory. 
 It is recommended to use a computer with III 400 MHz processor or higher, 
 XGA graphics and a Microsoft compatible mouse or an equivalent pointing device
 is required.
 
 Please also note the hardware requirements of device drivers.
 
===============================================================================
4. Installation
===============================================================================
 Under Windows 2000/XP/Vista Administrator Rights are required.

 Prior to installing PACTware to the computer, all running programs must be closed.
  .net Runtime Environment Version 1.1 including the service pack 1 must be installed on your PC.

 The Setup-File PACTware36setup.zip contains
 the Base-Setup for PACTware 3.6 with Online-Help in several languages
 the HART ComDTM for PACTware 3.6 the HART Scan Addin and the Generic HART DTM

 After unpacking the installation into a temporary directory it is started by a 
 double-click on Setup.exe.
 
 After selecting the installation language the user is guided through the installation.
 Optional components like e.g. the manuals cannot be installed in this process. 
 An individual setup is automatically starting for the HART ComDTM and the Generic HART DTM
 requesting user input.

 If PACTware 2.4, PACTware 3.0 or PACTware 3.5 were installed on the PC, all passwords for 
 PACTware 3.6 can be applied at the end of the installation. 

 Installation of PACTware 3.6 replaces PACTware 3.5 whereas PACTware 2.4 and PACTware 3.0 
 can be used on the same PC in parallel.

 A program group for the current user is entered to the Windows Start menu
 and a link to PACTware 3.6 is displayed on the desktop.

===============================================================================
5. Deinstallation
===============================================================================
 PACTware is deinstalled via menu item "Customize" in the program group
 named PACTware 3.6.
 
 Prior to starting the deinstallation program, PACTware must be exited,
 as otherwise it is impossible to deinstall all components.

===============================================================================
6. Start PACTware
===============================================================================
 PACTware is always delivered with at least one DTM. Before starting
 PACTware, the DTM and its setup program must have been installed.

 PACTware is either started by a double-click on the link on the desktop or in the Windows 
 Start menu via <Programs> in the installed program group using
 entry PACTware 3.6.

===============================================================================
7. Known Problems
===============================================================================
7.1 When PC is under remote control using tools like PCanywhere or VNC, 
PACTware menus are not displayed correct.

7.2 Parameter window of HART CommDTM should only be used in Tabbed MDI window mode.

7.3 If only the tree view of the device catalog is displayed under certain conditions, execution of  
PACTwareResetSettings.reg file delivered with the installation .zip file sets default width of 
the tree view subwindow again.

7.4 Only the left part of a print out of DTM parameters and project tree is shown with Microsoft internet 
explorer versions earlier than 7.0. Internet explorer version 7 provides a print out of all information.

7.5 Using Softing ComDTM release 2.04 without a valid license leads to a program stall during opening an 
existing project that includes this DTM. A valid license is required.

===============================================================================
8. Changes in this version
===============================================================================
8.1 PACTware 3.6 runs under Windows VISTA

8.2 Windows NT 4.0 not any longer supported

8.3 The TCI (Tool calling inerface) level 3 is provided

===============================================================================
9. Error messages
===============================================================================
 In case of  DTM- or PACTware-related problems, contact the hotline
 hotline@pactware.com or by phone 0180 5 350050 (12 ct/Min. out of german fixed network).

 Information about the vendor of PACTware is contained in a form, which is called 
 via menu item About in the help menu.

 Information about the DTM can be obtained either via menu item Properties
 by opening the context menu of the device in the project structure or via the Info key
 of after selecting the concerned device from the catalog. 

 Please state the operating system PACTware runs under as well as the PACTware 
 and DTM program versions. Any information about the interactions and/or the 
 implemented functions, which may have caused the problem, are appreciated 
 for trouble-shooting. In addition, screen shots are helpful in the analysis.

===============================================================================
10. Download .NET Framework 1.1 and .NET Framework 1.1 SP 1
===============================================================================
 Link to Download .NET Framework 1.1:
 http://www.microsoft.com/downloads/details.aspx?familyid=262D25E3-F589-4842-8157-034D1E7CF3A3&displaylang=en

 Link to Download .NET Framework 1.1 SP 1:
 http://www.microsoft.com/downloads/details.aspx?familyid=a8f5654f-088e-40b2-bbdb-a83353618b38&displaylang=en