Release Notes for Modbus Communication DTM Library V1.6


This document gives recommendations and provides additional information for installing and running the

 Communication DTM for Modbus Serial V2.0.1
 Communication DTM for Modbus TCP V2.0


1. System Platforms

The Modbus Communication DTM Library can be installed on different Windows platforms using the same setup package. The setup will detect the platform and the specific installation requirements automatically. The following Windows platforms are supported:
 Windows 2000 (Service Pack 3 and above)
 Windows XP Professional (Service Pack 2 and above)
 Windows Vista 32-Bit
 Windows Vista 64-Bit

In addition, the following system components are required:
 Microsoft.NET Framework 2.0
 FDT Frame Application compliant to FDT 1.2 or FDT 1.2.1 standard

The FDT Frame Application must support the Microsoft.NET Framework 2.0.


2. Minimum Resource Requirements

Please verify that the target system meets the following minimum requirements:
 processor type: Pentium III or equivalent
 processor speed: 500 MHz (800 MHz recommended)
 memory: 128 MB (256 MB recommended, Windows XP: 256 MB)
 display: 800x600, 256 colors (1024x768 recommended)
 free hard disk space on system drive: 30 MB
 free hard disk space on installation drive: 30 MB 
 swap file: 256 MB (512 MB recommended)
	

3. Installation Preparations
	
Executing the single setup file will extract the appropriate set of files onto the local hard drive. It will then start the installation automatically. Before starting the installation, please perform the following checks and preparations:
 Please close all running applications before starting the setup program.
 For the installation of the Modbus Communication DTM Library please ensure that you have logged in with a user ID having administrator privileges on operating system.
	
	
	
4. Installation Language

The language of the installation dialogs can be selected at the start of the installation.
	
	
5. Program Group
	
 The installation will not add any folder in the Programs group oft the Start menu because the 
Modbus Communication DTM Library can only be used inside an FDT Frame Application.
	
	
6. Directories
	
By default, Modbus Communication DTM Library Configuration Software will be installed in the directory
	
-<CommonProgramFiles>
	-Schneider Electric Shared
		-Schneider Electric Modbus Communication DTM Library
			- Modbus Serial Line CommDTM
			- Modbus TCP CommDTM
	
where <CommonProgramFiles> depends on the settings of your machine. 
In a default system installation, this directory is usually "C:\Program Files\Common Files\ ". 
The default setting can be modified at the time of installation to meet your specific requirements.


7. Uninstall, Modify, Repair

Invoking the installation procedure of the Modbus Communication DTM Library again will result in a slightly different way of presentation offering to uninstall, to modify, or to repair the existing setup.


8. Known Problems

This installation uses Microsoft Windows Installer technology version 2.0. If necessary, it will update your system at the beginning of the installation process. In this case, a reboot may be required.

The update will probably fail if the system is running Microsoft Windows Installer version 1.2.
In this case, please contact your system administrator to have the system settings corrected first.
The Microsoft Knowledge Base article 319624 provides additional information about potential causes of this problem (http://support.microsoft.com/?kbid=319624).