﻿===============================================================================
|                                                                             |
|     VisuNet RM Shell 5.5.1.1200                                             |
|     18-33556N                                                               |
|                                                                             |
===============================================================================
|                                                                             |
|     Pepperl+Fuchs SE                                                        |
|     Innovation Unit HMI                                                     |
|     20. Aug. 2021                                                           |
|                                                                             |
===============================================================================

====================
Release: 18-33556N
Version: 5.5.1.1200
Date:    20-AUG-2021
====================

  Improved:
  ----------
   #FR-1696: Emerson DRDC updated to 3.3.3.
   #FR-1721: Chromium (CefSharp) updated to 91.1.230.0.
   #3030:    Secure Tunnel now supports TLS protocol TLS1.1 and newer.

  Bug fixes:
  ----------
   #1892:    Dialog Filter: Window Service does not refresh whitelist status of open Windows.
   #1926:    System Tools: Cannot open another Log File.
   #2957:    Previs: PIN field does not accept space input anymore.
   #2958:    Previs: Previs does not block input after device restart.
   #3020:    Hide Windows internal Network Adapters in Shell network tab.
   #3049:    Fixed black screen when trying to perform a reboot or shutdown with enabled Write Filter.
   #3059:    Fixed missing DRDC services after update from Shell 5.0.3.
   #3060:    Updated Log4Net to 2.0.12 (NVD - CVE-2018-1285 (nist.gov)).
   #3066:    Updated GXP SC_Service to 1.4.1.346.
   #3071:    Fixed warning that Ngen couldn't find IWshRuntimeLibrary.


====================
Release: 18-33556M
Version: 5.5.0.1166
Date:    14-DEC-2020
====================

  New Features:
  -------------
   #FR-1462: Wedge App, System Tools App and IP Address in About Tile can now be hidden from Operator.
   #FR-1491: Added Disk Cleanup Service.
   #2669:    Quad monitor setup with square 2x2 layout can be aligned automatically.
   #2883:    Updated DRDC to version 3.3.1.1125 (DeltaV 3.3.3).

  Improved:
  ----------
   #2360:    Windows Virtual Memory (Pagefile) is enabled again after Write Filter was disabled.
   #2562:    Renamed "USB pen drive" to "USB Flash Drive" in Update view.
   #2637:    Renamed "Brightness Button" to "Brightness Buttons" in GXP Frontkey Settings view.
   #2843:    Factory Reset password is not required to be changed  in First Start Wizard when it was changed before.
   #2936:    RM Shell Updates now support additional setup information and description.
   #2946:    Floating OSK Button is now started directly after it is enabled and does not require a restart anymore.
   #2948:    Obsolete update files will be deleted when not used anymore.
   #2962:    Manually deleted files will be deleted directly without using the Windows Recycle Bin (Group Policy Setting).
   #2964:    Temporary update files will be deleted when prerequisites are not met or when the update fails.
   #2965:    Updates cannot be (accidently) deleted anymore from external USB Flash Drives or network folders using the RM Shell Update View.
   #2980:    Floating OSK Button may not be visible on displays with Scale setting > 100%.

  Bug fixes:
  ----------
   #2537:    Profiles will not start anymore in Engineer or Administrator role when uploaded by VisuNet CC.
   #2994:    On-Screen-Keyboard caused a crash of the RM Shell after Windows 10 Security Update 11-2020(18-33624K) was installed.


====================
Release: 18-33556L
Version: 5.4.1.1032
Date:    16-SEP-2020
====================

  Improved:
  ----------
    #2859: Add Support for calibrating touch sensitivity for new eGalax touch controller (Orion series)
    #2860: Add Support for the mouse mode of new eGalax touch controller (Orion series)
    #2865: Keyboard Layout now visible inside OOBE screen

  Bug fixes:
  ----------
    #2862: Multi-Monitor Setup with different DPI settings caused a missing button inside the connection tab.
    #2874: Set Region button inside the OOBE screen opened wrong Windows Settings Page.

====================
Release: 18-33556K
Version: 5.4.0.986
Date:    03-AUG-2020
====================

  New Features:
  -------------
    #2783: Added Support for Windows 10 LTSC 2019

  Improved:
  ----------
    #2788: Shell startup and loading operation screen improved
    #2693: Updated GXP SC Service to Version 1.4.0.304 with improved startup and reset behavior
    #2833: Sequential loading of the home screen functions to increase the stability and performance

  Bug fixes:
  ----------
    #2785: In case of no available Factory Reset on a device, data could not be downloaded via VisuNet CC. 
    #2796: Disabling Cursor Blink caused a very fast blinking cursor.
    #2804: Adaption of .Net version in About screen.
    #2834: The Windows User Autologin for devices, that were cloned was fixed.
    #2832: RDP sometimes showed an error message after the connection was closed.
    #2827: DRDC info was shown in About even if there was no DRDC license available.
    #2826: Devices with Bluetooth or Wifi modules, that are using the capture or apply mechanism with VisuNet Control Center are supported now.

====================
Release: 18-33556J
Version: 5.3.0.928
Date:    15-MAY-2020
====================

  New Features:
  -------------
    Support for Factory Reset 6.0.
    #FR-1232: Factory Reset password options: You can change the Factory Reset password inside the System Settings/Security Tab. Additionally, you can change the Factory Reset password inside the First Start Wizard.

====================
Release: 18-33556H
Version: 5.2.0.910
Date:    20-MAR-2020
====================

  Bug fixes:
  ----------
    #2663: Device is not shutting down in First start Menu and OOBE
    #2668: Maintenance Mode overlay may not be closed due to late watchog initialization

====================
Release: 18-33556G
Version: 5.2.0.900
Date:    19-FEB-2020
====================

  New Features:
  -------------
    #FR-878:  Added a login prompt (PIN) for Previs
    #FR-1166: Added support for the new Raritan KVM IV 
    #FR-1182: Improved the installation process for Raritan KVM adapters
    #FR-1312: Added PenTouch support

  Improved:
  ----------
    #2546: First start wizard asks user for restart when computer name was changed
    #2567: GXP: Show I2C Warnings in the About screen
    #2570: Updated DRDC to 3.3.2
    #2571: Updated CefSharp to 75.1.143.0

  Bug fixes:
  ----------
    #2581: Fixed Certificate settings in Group Policy

====================
Release: 18-33556F
Version: 5.1.1.802
Date:    24-SEP-2019
====================

  Bug fixes:
  ----------
    #2550: Fixed crash of the Shell after reboot when only DRDC license entered.


====================
Release: 18-33556E
Version: 5.1.0.787
Date:    13-SEP-2019
====================

  New Features:
  -------------
    #FR-550: Added Secure SSL Connection for Session Shadowing/Desktop Sharing
    #FR-554: Added OOBE Setup Wizard
    #FR-1035: Re-align / refresh monitor orientation after incidental monitor turn off/on
    #2441: Desktop Sharing Server is now usable without Pro or CC License.


  Improved:
  ---------
    #1870: Improved setting up display resolution.
    #2135: Provide RM Image and Factory Reset information to VisuNet Control Center.
    #2163: RDP client runs in a separte process to improve stability and performance.
    #2179: Updated to CefSharp (Chromium) 71.0
    #2196: Updated to S-Code VNC Viewer 3.8.3
    #2197: Update to TightVNC Server 2.8.11.
    #2223: Improved RDP monitor allignement after a monitor is reconnected.
    #2244: GXP/IXD Touch: Show only two sensitivity modes.
    #2248: Improved version handling for connection profiles using VisuNet Control Center.
    #2276: "Taskmanager" is now "Task Switcher".
    #2298: Improved validation of IP adresses.
    #2310: Closing a profile within the Profile Management does not require two clicks anymore.
    #2346: Cleaned the user interface of the profile setting pages.
    #2352: Removed disconnect messages for user initiated disconnects.
    #2353: Added timestamp to notifications.
    #2354: Renamed "GXP Touch" to "eGalaxTouch", because it is used in different devices.
    #2355: Improved notifications and only show new ones.
    #2358: Improved 4k support with various DPI settings.
    #2389: Improved restart mechanism after a crash of the Shell.
    #2391: Removed security critical functions from service menu.
    #2392: Added progressive delay to enter the service menu when login failed.
    #2421: Improved error Messages for Raraitan KVM.
    #2429: Renamed "Pepperl+Fuchs GmbH" to "Pepperl+Fuchs AG"
    #2456: Removed the host file editor.
    #2457: Improved setting static IP adresses on disconnected network adapters.
    #2461: Added information page when chromium couldn't load a webpage.
    #2468: Added audio redirection settings for RDP connections. RDP audio redirection is disabled by default now.
    #2470: Disabled audio redirection by default in DRDC profiles.
    #2499: Updated Group Policies and added parts of the Microsoft Security Baseline (Update).


  Bug fixes:
  ----------
    #2173: Fixed certificate import with private password using VisuNet Control Center.
    #2232: Fixed network connection interruption when settings uploaded using VisuNet Control Center.
    #2270: Fixed losing profile settings (auto reconnect, connection backup and retry settings) when the device was configured using Visuâ€¦â€�
    #2273: Fixed Shell freeze when Task Switcher was opened while starting an RDP profile.
    #2279: Fixed losing Shell configuration after restart when configured using VisuNet Control Center.
    #2293: Fixed continously running ping of DRDC server even if connection was closed.
    #2302: Fixed loosing Generic App Icons after uploading device settings with VisuNet Control Center.
    #2315: Fixed resizing issue at desktop sharing profile when profile is reopened from Shell.
    #2320: Fixed possible crash when VNC client was closed when authentication window is visible.
    #2332: The Raritan KVM Remote Console window was not closed.
    #2345: Fixed missing connection bar setting for Raritan KVM profile.
    #2367: Fixed possible Shell crash when display scale > 150% and using VisuNet Control Center.
    #2384: Fixed loosing DRDC Tcp redundancy settings after a RM Shell update.
    #2472: RM Shell now sends correct certificate store names to VisuNet Control Center.


  Known Issues:
  -------------
    #1754: DRDC: SSL Certificate - Controls backdoor security issue
    #2422: VNC: No error message when VNC connection closed by server disconnection
    #2423: After removing the main display and reconnect it the connection bar has the wrong size
    #2448: RDP: Windows Position after open System Settings (mixed monitor setup)
    #2459: IE: Window not maximized again when one monitor was disconnected/connected
    #2460: Chrome: Window not maximized again when one monitor was disconnected/connected
    #2481: Update: Portable USB Drive (SSD) does not work for Update


==================
Release: 18-33556D
Version: 5.0.3.597
==================

  Bug fixes:
  ----------
    #2212: Update DRDC to 3.3.1
    #2221: The Shell crashes if you want to call the Taskmanager while connecting to an RDP profile.


==================
Release: 18-33556C
Version: 5.0.2.575
==================

  Improved:
  ---------
    #2136: Updated DRDC to 3.3.0.20 (Hotfix 3)
    #2139: DRDC connect and reconnect mechanism improved. Asynchronous pattern used.
    #2119: Windows Service management from Shell improved

  Bug fixes:
  ----------
    #2158: DRDC could crash when Auto-Reconnect is enabled, but server is not reachable (GDI handles leak)
    #2115: Input Language was not updated in OOBE dialog
    #2181: Removed incorrect sensitivity mode for IXD 19" and GXP 19" touch screen
    #2110: Shell could crash if custom App path is invalid and Autostart is enabled.
    #2159: KMSwitch: Mouse cursor not visible on slave system on GXP systems or when no pointing device connected


==================
Release: 18-33556B
Version: 5.0.1.441
==================

  Added:
  ------
    #1897: GXP - Mouse emulation mode for the touch screen
    #2014: GXP and IXD â€“ Keypad lock mechanism to prevent false button activation
    #2057: GXP - User can disable brightness buttons
    #2066: Desktop sharing password can be reset now


  Improved:
  ---------
    #2006: Made the RM Shell icon in the Taskswitcher less prominent and added keyboard shortcuts
    #2056: Updated Service Controller Service to 1.2.0.154
    #2058: VNC will redirect CTRL+ALT+DEL to CTRL+ALT+END for the host system
    #2059: Serial number is now write protected when a number has been added in production
    #2060: System Settings are refreshed when License key was entered
    #2061: Updated S2KWedge to Version 5.0.2.538
    #2069: Update Wrapper now shows free disk space, ram and cpu usage
    #2087: Title in Taskswitcher is now multiline
    #2093: Updated Update Wrapper to 5.0.0.441	


  Bug fixes:
  ----------
    #1920: GXP - Clean Lock does not ignore touch input
    #1938: Scheduler ignored system time format
    #1947: Updated EULA and 3rd party licenses
    #1995: Device not found using CC when Ethernet connected after the device was started
    #2004: RM Shell could be started multiple times
    #2018: Connection retry not working when first connection attemp failed
    #2043: Engineer can now calibrate ELO Touch screens
    #2044: Identify Display doesn't work when display scaling was > 100%
    #2050: Scroll function on Keyboard is activated when Shell Hotkey Alt+Ctrl+Scroll was pressed
    #2051: Taskswitcher Previews drawn on the wrong position when display scaling > 100%
    #2052: VisuNetCC Service could fail when network connection is instable
    #2063: Engineer could change the Dialog Filter (disabled now)
    #2075: OSK Overlay icon hides input text
    #2081: Ctrl+Alt+Tab not working for Administrator
    #2085: Dialog Filter settings editable even when write filter active
    #2090: Write Filter was set to RAM - is now DISK
    #2091: Remote and Advanced Windows Settings and Explorer context menu not accessible
    

==================
Release: 18-33556A
Version: 5.0.0.361
==================

  Bug fixes:
  ----------
    #1949: ELO Touch compatibility with RM Shell 5

    
==================
Release: 18-33556
Version: 5.0.0.341
==================

  New Features:
  -------------
    #FR-541: Added Active Directory support
    #FR-552: New License keys (Pro, CC, DRDC)
    #FR-562: Windows 10 IoT 2016 LTSB Enterprise x64
    #FR-564: Update to .Net 4.7
    #FR-587: Update to Internet Explorer 11
    #FR-591: Improve Shell Update mechanism
    #FR-593: Update to DevExpress 17.x
    #FR-690: Improve Update upload
    #FR-720: Improve Dialog Filter (as replacement for Keyboard Filter)
    #FR-723: MBR Filter
    #FR-724: Unified Write Filter (UWF)
    #FR-725: Write Filter UI integration
    #FR-727: Improve service access code
    #FR-734: Remove Volume Mixer
    #FR-735: Remove Citrix from Shell 5
    #FR-733: Generic App Management
    #FR-793: Scheduler for 24/7 operation
    #FR-794: Automatic restart when write filter memory is critical
    #FR-795: Windows Explorer Access
    #1854:   Update to DRDC 3.3.0.4
    #1855:   GXP: Allow disabling Brightness buttons
    #1780:   Netc@p is now a feature in the standard setup
    
  
  Bug fixes:
  ----------
    #1824: RDP: When RDP connection is idle for a given period the connection is closed
    #1729: DRDC: Liveness check fixed
    
  
  Known Issue:
  ------------
    #1759: TabTip: OSK can overlay the textedit
    #1939: EULA: License references to Windows 7 Standard
    #1870: System Settings: Display - Cannot change resolution to 1080P
    #1892: Dialog Filter: Window Service do not refresh whitelist status of open Windows.
    #1894: System Settings: Open Profile overlays Explorer
    #1920: System Tools: Clean Lock do not block GXP Touchscreen
    #1938: Scheduler: Time format is always 24h => use system time format
    #1841: Closing a DRDC connection cannot be canceled by the user
    #1840: DRDC shows two credential dialogs when no user and password credentials are stored
    #1891: RDP freezes when credentials dialog is clicked with touchscreen