Version: V1.00.001Release Date: 2023-03-02

This IODD is not valid - please run the IODD Checker!

Line 497, column 10: StdEventRef code=25424 not in StandardDefinitions


VMA-2+P-0,2M-PUR-IO-V1-G
Vendor ID 1 (0x0001) Vendor Logo
Vendor Name Pepperl+Fuchs
Vendor Text Pepperl+Fuchs
Vendor URL http://www.pepperl-fuchs.com/io-link
Device ID 984833 (0x0f0701)
DeviceFamily IO-Link Valve Connector
Features
Block Parameter yes
Data Storage yes
Profile Characteristic 0x4000 (Common Application Profile: Identification and Diagnosis)
Supported Access Locks Parameter: no, Data Storage: yes, Local Parameterization: no, Local User Interface: no
Communication
IO-Link Revision V1.1
Transmission Rate38400 bit/s (COM2)
Minimum Cycle Time 2.8 ms
SIO Mode Supported no
M-Sequence CapabilityPREOPERATE = TYPE_1_V with 8 octets on-request data
OPERATE = TYPE_2_V with 2 octets on-request data
ISDU supported
Device Variant VMA-2+P-0,2M-PUR-IO-V1-G
Description IO-Link Valve Connector, Form A, 2+P, PUR cable, M12 plug, 3-pin
Product ID 70142132
Device Icon Device Icon
Device Symbol Device Symbol
Connection TypeNon-standard connector
Connection Symbol Connection Symbol
Connection Description Plug, M12, 3-pin
- pin 1 brown; L+; Brown - L+
- pin 3 (light) blue; L-; Blue - L-
- pin 4 black; C/Q; Black - C/Q

ProcessData id=P_ProcessData

ProcessDataIn "PD Input" id=PI_PDin

bit length: 8
data type: 8-bit Record (subindex access not supported)

subindex bit offset data type allowed values default value acc. restr. mod. other var. excl. from DS name description
1 0 Boolean false = Off, true = On Valve Status Indicates the current status of the valve.
2 1 7-bit UInteger 0, 10..100 PWM Value Shows the current PWM value for the valve current.
Octet 0
bit offset 7 6 5 4 3 2 1 0
subindex 2 1
element bit 6 5 4 3 2 1 0  

ProcessDataOut "PD Output" id=PO_PDout

bit length: 8
data type: 8-bit Record (subindex access not supported)

subindex bit offset data type allowed values default value acc. restr. mod. other var. excl. from DS name description
1 0 Boolean false = Off, true = On Valve Control Controls the on/off status of the valve.
2 1 7-bit UInteger 0, 10..100 PWM Control Sets the PWM value for the valve current. If the value is 10 or less, the defined value in the parameter PWM Value is applied.
Octet 0
bit offset 7 6 5 4 3 2 1 0
subindex 2 1
element bit 6 5 4 3 2 1 0  

Standard Variable "Direct Parameters - Page 1" index=0 id=V_DirectParameters_1

description: Comprises the required parameters defining the communication characteristics and identifiers for device validation.
data type: 128-bit Record
access rights: rw

subindex bit offset data type allowed values default value acc. restr. mod. other var. excl. from DS name description
1 120 8-bit UInteger ro Reserved
2 112 8-bit UInteger ro Master Cycle Time Communication: Current communication cycle duration used by the master. This value defines the process data cycle.
3 104 8-bit UInteger ro Min Cycle Time Communication: Minimum communication cycle duration supported by the device. This value defines the lowest possible process data cycle.
4 96 8-bit UInteger ro M-Sequence Capability Communication: Information on the structure and the supported features of the communication messages.
5 88 8-bit UInteger 17 ro IO-Link Revision ID Communication: Identifier for the currently used communication protocol revision.
6 80 8-bit UInteger ro Process Data Input Length Communication: Information on width and features of the process input data (Process Data from Device to Master).
7 72 8-bit UInteger ro Process Data Output Length Communication: Information on width of the process output data (Process Data from Master to Device).
8 64 8-bit UInteger ro Vendor ID 1 Identification: Highest octet of the Vendor ID. Combined with the parameter Vendor ID 2, this parameter defines the 16-bit value of the unique Vendor ID as assigned by the IO-Link Community.
9 56 8-bit UInteger ro Vendor ID 2 Identification: Lowest octet of the Vendor ID. Combined with the parameter Vendor ID 1, this parameter defines the 16-bit value of the unique Vendor ID as assigned by the IO-Link Community.
10 48 8-bit UInteger ro Device ID 1 Identification: Highest octet of the Device ID. Combined with the parameters Device ID 2 and 3, this parameter defines the 24-bit value of the vendor-specific Device ID.
11 40 8-bit UInteger ro Device ID 2 Identification: Middle octet of the Device ID. Combined with the parameters Device ID 1 and 3, this parameter defines the 24-bit value of the vendor-specific Device ID.
12 32 8-bit UInteger ro Device ID 3 Identification: Lowest octet of the Device ID. Combined with the parameters Device ID 1 and 2, this parameter defines the 24-bit value of the vendor-specific Device ID.
13 24 8-bit UInteger ro Reserved
14 16 8-bit UInteger ro Reserved
15 8 8-bit UInteger ro Reserved
16 0 8-bit UInteger wo X System Command Application: Command interface for devices without ISDU support. Validity and execution of commands are not confirmed.
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
Standard Variable "Direct Parameters - Page 2" index=1 id=V_DirectParameters_2

description: A set of parameters for devices without ISDU support.
data type: 128-bit Record
access rights: rw

subindex bit offset data type allowed values default value acc. restr. mod. other var. excl. from DS name description
1 120 8-bit UInteger Device-specific Parameter 1
2 112 8-bit UInteger Device-specific Parameter 2
3 104 8-bit UInteger Device-specific Parameter 3
4 96 8-bit UInteger Device-specific Parameter 4
5 88 8-bit UInteger Device-specific Parameter 5
6 80 8-bit UInteger Device-specific Parameter 6
7 72 8-bit UInteger Device-specific Parameter 7
8 64 8-bit UInteger Device-specific Parameter 8
9 56 8-bit UInteger Device-specific Parameter 9
10 48 8-bit UInteger Device-specific Parameter 10
11 40 8-bit UInteger Device-specific Parameter 11
12 32 8-bit UInteger Device-specific Parameter 12
13 24 8-bit UInteger Device-specific Parameter 13
14 16 8-bit UInteger Device-specific Parameter 14
15 8 8-bit UInteger Device-specific Parameter 15
16 0 8-bit UInteger Device-specific Parameter 16
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
description: Command interface for applications. A positive acknowledge indicates the complete and correct finalization of the requested function.
data type: 8-bit UInteger
allowed values: 129 = Application Reset, 130 = Restore Factory Settings
access rights: wo
modifies other variables

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Standard Variable "Device Access Locks" index=12 id=V_DeviceAccessLocks

description: The access to the device parameters can be restricted by setting appropriate flags within this parameter.
data type: 16-bit Record (subindex access not supported)
access rights: rw

subindex bit offset data type allowed values default value acc. restr. mod. other var. excl. from DS name description
1 0 Boolean false = Unlocked, true = Locked Parameter Write Access This lock prevents the write access to all read/write parameters of the device except for the parameter 'Device Access Locks'.
2 1 Boolean false = Unlocked, true = Locked 0 Data Storage This lock prevents the write access to the device parameters via the data storage mechanism.
3 2 Boolean false = Unlocked, true = Locked Local Parameterization This lock prevents the device settings from being changed via local operating elements on the device.
4 3 Boolean false = Unlocked, true = Locked Local User Interface This lock prevents the access to the device settings and display via a local user interface. The user interface is disabled.
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
description: The vendor name that is assigned to a Vendor ID.
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
description: Additional information about the vendor.
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
description: Complete product name.
data type: 64-octet String UTF-8
default value: "VMA-2+P-0,2M-PUR-IO-V1-G"
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
description: Vendor-specific product or type identification (e.g., item number or model number).
data type: 64-octet String UTF-8
default value: "70142132"
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
description: Additional product information for the device.
data type: 64-octet String UTF-8
default value: "IO-Link Valve Connector"
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
description: Unique, vendor-specific identifier of the individual device.
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
Standard Variable "Hardware Revision" index=22 id=V_HardwareRevision

description: Unique, vendor-specific identifier of the hardware revision of the individual device.
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
Standard Variable "Firmware Revision" index=23 id=V_FirmwareRevision

description: Unique, vendor-specific identifier of the firmware revision of the individual device.
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
Standard Variable "Application-specific Tag" index=24 id=V_ApplicationSpecificTag

description: Possibility to mark a device with user- or application-specific information.
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
description: Indicator for the current device condition and diagnosis state.
data type: 8-bit UInteger
allowed values: 0 = Device is OK, 1 = Maintenance required, 2 = Out of specification, 3 = Functional check, 4 = Failure
default value: 0
access rights: ro
dynamic

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Standard Variable "Detailed Device Status" index=37 id=V_DetailedDeviceStatus

description: List of all currently pending events in the device.
data type: Array[3] of 3-octet OctetString (subindex access not supported)
access rights: ro
dynamic

octet 0 1 2 3 4 5 6 7
bit offset 71 - 64 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8
subindex 1 1 1 2 2 2 3 3

octet 8  
bit offset 7 - 0  
subindex 3  

Variable "Function Tag" index=25 id=V_CP_FunctionTag

description: Possibility to mark a device with function-specific information.
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
Variable "Location Tag" index=26 id=V_CP_LocationTag

description: Possibility to mark a device with location-specific information.
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
Variable "Valve Operation Mode" index=77 id=V_XPFA_VMA_Mode

description: Selects between different modes of operation for the valve connector.
data type: 8-bit UInteger
allowed values: 0 = Smart, 1 = Standard, 2 = On/off sequence, 3 = Off/on sequence, 4 = Off/on delay, 5 = On/off delay
default value: 0
access rights: rw

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Variable "Valve On Time" index=78 id=V_XPFA_VMA_TimerOn

description: Defines the delay time for the valve to turn on after being triggered.
data type: 16-bit UInteger
allowed values: 0..65535
default value: 1
access rights: rw

octet 0 1  
bit offset 15 - 8 7 - 0  
element bit 15 - 8 7 - 0  

Variable "Valve Off Time" index=79 id=V_XPFA_VMA_TimerOff

description: Defines the delay time for the valve to turn off after being triggered.
data type: 16-bit UInteger
allowed values: 0..65535
default value: 9
access rights: rw

octet 0 1  
bit offset 15 - 8 7 - 0  
element bit 15 - 8 7 - 0  

Variable "Switching Cycles Absolute" index=80 id=V_XPFA_VMA_MonCounterAbs

description: Shows the absolute number of valve switching cycles since initial commissioning.
data type: 32-bit UInteger
allowed values: 0..4294967295
access rights: ro
dynamic

octet 0 1 2 3  
bit offset 31 - 24 23 - 16 15 - 8 7 - 0  
element bit 31 - 24 23 - 16 15 - 8 7 - 0  

Variable "Switching Cycles Limit Absolute" index=81 id=V_XPFA_VMA_ConfigCounterAbs

description: Defines the limit of valve switching cycles since initial commissioning. If the limit is exceeded the according status flag in the parameter Diagnosis Status is set.
data type: 32-bit UInteger
allowed values: 0..4294967295
default value: 10000000
access rights: rw

octet 0 1 2 3  
bit offset 31 - 24 23 - 16 15 - 8 7 - 0  
element bit 31 - 24 23 - 16 15 - 8 7 - 0  

Variable "Switching Cycles Relative" index=82 id=V_XPFA_VMA_MonCounterRel

description: Shows the number of valve switching cycles since the last application reset, restore to factory settings or manual reset of the value.
data type: 32-bit UInteger
allowed values: 0..4294967295
default value: 0
access rights: rw
dynamic

octet 0 1 2 3  
bit offset 31 - 24 23 - 16 15 - 8 7 - 0  
element bit 31 - 24 23 - 16 15 - 8 7 - 0  

Variable "Switching Cycle Limit Relative" index=83 id=V_XPFA_VMA_ConfigCounterRel

description: Defines the limit of valve switching cycles since the last application reset, restore to factory settings or manual reset of the value. If the limit is exceeded the according status flag in the parameter Diagnosis Status is set.
data type: 32-bit UInteger
allowed values: 0..4294967295
default value: 2000000
access rights: rw

octet 0 1 2 3  
bit offset 31 - 24 23 - 16 15 - 8 7 - 0  
element bit 31 - 24 23 - 16 15 - 8 7 - 0  

Variable "Supply Voltage" index=100 id=V_XPFA_VMA_MonSupplyVoltage

description: Shows the current supply voltage of the device.
data type: 8-bit UInteger
allowed values: 0..255
access rights: ro
dynamic

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Variable "On Resistance" index=101 id=V_XPFA_VMA_MonOnResistance

description: Shows the current on resistance of the valve.
data type: 16-bit UInteger
allowed values: 0..65535
access rights: ro
dynamic

octet 0 1  
bit offset 15 - 8 7 - 0  
element bit 15 - 8 7 - 0  

Variable "PWM Value" index=102 id=V_XPFA_VMA_ConfigPWM

description: Defines the mark-space ratio of the PWM modulated valve current in percent.
data type: 8-bit UInteger
allowed values: 10..100
default value: 50
access rights: rw

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Variable "Pick-up Time" index=103 id=V_XPFA_VMA_ConfigPickupTime

description: Defines the pick-up time of the valve current.
data type: 16-bit UInteger
allowed values: 5..2000
default value: 150
access rights: rw

octet 0 1  
bit offset 15 - 8 7 - 0  
element bit 15 - 8 7 - 0  

Variable "Switching Time" index=104 id=V_XPFA_VMA_MonSwitchingTime

description: Shows the time for the valve to switch on.
data type: 16-bit UInteger
allowed values: 0..65535
access rights: ro
dynamic

octet 0 1  
bit offset 15 - 8 7 - 0  
element bit 15 - 8 7 - 0  

Variable "Valve Current" index=105 id=V_XPFA_VMA_MonValveCurrent

description: Shows the supply current of the valve.
data type: 16-bit UInteger
allowed values: 0..65535
access rights: ro
dynamic

octet 0 1  
bit offset 15 - 8 7 - 0  
element bit 15 - 8 7 - 0  

Variable "Valve Current Limit" index=106 id=V_XPFA_VMA_ConfigCurrentLimit

description: Defines a threshold for the valve current. If this limit is exceeded the according status flag in the parameter Diagnosis Status is set.
data type: 16-bit UInteger
allowed values: 0..1100
default value: 600
access rights: rw

octet 0 1  
bit offset 15 - 8 7 - 0  
element bit 15 - 8 7 - 0  

Variable "Valve Power" index=107 id=V_XPFA_VMA_MonValvePower

description: Shows the current power dissipation of the valve.
data type: 16-bit UInteger
allowed values: 0..65535
access rights: ro
dynamic

octet 0 1  
bit offset 15 - 8 7 - 0  
element bit 15 - 8 7 - 0  

Variable "Temperature" index=108 id=V_XPFA_VMA_MonTempCur

description: Shows the currently observed operating temperature of the connector.
data type: 16-bit Integer
allowed values: -100..200
access rights: ro
dynamic

octet 0 1  
bit offset 15 - 8 7 - 0  
element bit 15 - 8 7 - 0  

Variable "Temperature Limit" index=109 id=V_XPFA_VMA_ConfigTempLimit

description: Defines a maximum temperature threshold for the device operation. If the limit is exceeded the according status flag in the parameter Diagnosis Status is set.
data type: 16-bit Integer
allowed values: -100..200
default value: 85
access rights: rw

octet 0 1  
bit offset 15 - 8 7 - 0  
element bit 15 - 8 7 - 0  

Variable "Overtemperature Exceeded Counter" index=110 id=V_XPFS_VMA_MonTempExceedCount

description: Shows the number of overtemperature incident with operating temperatures above the configured temperature limit.
data type: 16-bit UInteger
allowed values: 0..65535
access rights: ro
dynamic

octet 0 1  
bit offset 15 - 8 7 - 0  
element bit 15 - 8 7 - 0  

Variable "Maximum Operating Temperature" index=111 id=V_XPFA_VMA_MonTempMax

description: Shows the maximum observed temperature in powered operation since the last reset of the maximum value.
data type: 16-bit Integer
allowed values: -100..200
access rights: ro
dynamic

octet 0 1  
bit offset 15 - 8 7 - 0  
element bit 15 - 8 7 - 0  

Variable "Maximum Temperature Reset" index=112 id=V_XPFA_VMA_Cmd

description: Provides a command interface.
data type: 8-bit UInteger
allowed values: 0, 1 = Maximum Temperature Reset
access rights: wo

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Variable "Indication Mode" index=113 id=V_XPFA_VMA_IndicationMode

description: Selects the indication mode for the LED to either communication state or state of the valve.
data type: 8-bit UInteger
allowed values: 0 = Valve state, 1 = Communication state
default value: 0
access rights: rw

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Variable "LED Color Off" index=114 id=V_XPFA_VMA_LedColorOff

description: Selects the color of the LED for indication of an off-state.
data type: 8-bit UInteger
allowed values: 0 = Off, 1 = Blue, 2 = Green, 3 = Cyan, 4 = Red, 5 = Magenta, 6 = Yellow, 7 = White
default value: 2
access rights: rw

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Variable "LED Color On" index=115 id=V_XPFA_VMA_LedColorOn

description: Selects the color of the LED for indication of an on-state.
data type: 8-bit UInteger
allowed values: 0 = Off, 1 = Blue, 2 = Green, 3 = Cyan, 4 = Red, 5 = Magenta, 6 = Yellow, 7 = White
default value: 6
access rights: rw

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Variable "LED Color Warning" index=116 id=V_XPFA_VMA_LedColorWarn

description: Selects the color of the LED for indication of a pending warning.
data type: 8-bit UInteger
allowed values: 0 = Off, 1 = Blue, 2 = Green, 3 = Cyan, 4 = Red, 5 = Magenta, 6 = Yellow, 7 = White
default value: 4
access rights: rw

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Variable "LED Mode Warning" index=117 id=V_XPFA_VMA_LedModeWarn

description: Selects the indication mode of the LED for a pending warning to either constantly on or blinking.
data type: 8-bit UInteger
allowed values: 0 = Constant, 1 = Blinking
default value: 1
access rights: rw

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Variable "Locator Indication" index=118 id=V_XPFA_VMA_Locator

description: If enabled, the LED shows a specific blink pattern in order to better spot the device amongst other similar devices.
data type: 8-bit UInteger
allowed values: 0 = Disabled, 1 = Enabled
default value: 0
access rights: rw

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Variable "Event Configuration" index=119 id=V_XPFA_VMA_ConfigEvent

description: Enables triggering of events from available event sources if an according incident is detected.
data type: 8-bit UInteger
allowed values: 0 = Disabled, 1 = Enabled
default value: 0
access rights: rw

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Variable "Diagnosis Status" index=120 id=V_XPFA_VMA_DiagStatus

description: Shows the diagnosis states for different incident channels.
data type: 16-bit Record (subindex access not supported)
access rights: ro
dynamic

subindex bit offset data type allowed values default value acc. restr. mod. other var. excl. from DS name description
1 0 Boolean false = Inactive, true = Active Switching Cycles Absolute Overflow Indicates that the number of switching cycles since initial commissioning has exceeded the configured limit. Check or replace valve and connector.
2 1 Boolean false = Inactive, true = Active Switching Cycles Relative Overflow Indicates that the number of switching cycles since the last application reset, restore to factory settings or manual reset has exceeded the configured limit. Check or replace valve and connector.
3 2 Boolean false = Inactive, true = Active Temperature Underrun Indicates that the temperature has dropped below the specified limit.
4 3 Boolean false = Inactive, true = Active Temperature Overrun Indicates that the temperature has exceeded the configured limit.
5 4 Boolean false = Inactive, true = Active Valve Switching Alarm Indicates that the valve didn't switch within the expected time.
9 8 Boolean false = Inactive, true = Active Supply Undervoltage Indicates that the supply voltage is below the specified limit.
10 9 Boolean false = Inactive, true = Active Supply Overvoltage Indicates that the supply voltage is above the specified limit.
11 10 Boolean false = Inactive, true = Active Powersupply Fault Indicates that the supply voltage is out of the specified range.
12 11 Boolean false = Inactive, true = Active Overheat Fault Indicates that the device is overheated due to load or ambient conditions.
13 12 Boolean false = Inactive, true = Active Open Circuit Fault Indicates that the connection to the valve is interrupted.
14 13 Boolean false = Inactive, true = Active Current Overload Indicates that the detected load on the valve connector is too high.
15 14 Boolean false = Inactive, true = Active Short Circuit Indicates that a short circuit is detected at the valve connector.
Octet 0
bit offset 15 14 13 12 11 10 9 8
subindex / / / / / / 15 14 13 12 11 10 9
Octet 1
bit offset 7 6 5 4 3 2 1 0
subindex / / / / / / / / / / / / / / / / / / 5 4 3 2 1

Variable "Fail Safe State" index=121 id=V_XPFA_VMA_ConfigFailSafe

description: Defines the target state of the valve if any failure is detected.
data type: 8-bit UInteger
allowed values: 0 = Off, 1 = Hold
default value: 0
access rights: rw

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Variable "Product URI" index=191 id=V_XPFS_ProductURI

description: Provides an unique instance identification compliant to DIN-SPEC 91406.
data type: 100-octet String US_ASCII
access rights: ro

octet 0 1 2 3 4 5 6 7
bit offset 799 - 792 791 - 784 783 - 776 775 - 768 767 - 760 759 - 752 751 - 744 743 - 736

octet 8 9 10 11 12 13 14 15
bit offset 735 - 728 727 - 720 719 - 712 711 - 704 703 - 696 695 - 688 687 - 680 679 - 672

octet 16 17 18 19 20 21 22 23
bit offset 671 - 664 663 - 656 655 - 648 647 - 640 639 - 632 631 - 624 623 - 616 615 - 608

octet 24 25 26 27 28 29 30 31
bit offset 607 - 600 599 - 592 591 - 584 583 - 576 575 - 568 567 - 560 559 - 552 551 - 544

octet 32 33 34 35 36 37 38 39
bit offset 543 - 536 535 - 528 527 - 520 519 - 512 511 - 504 503 - 496 495 - 488 487 - 480

octet 40 41 42 43 44 45 46 47
bit offset 479 - 472 471 - 464 463 - 456 455 - 448 447 - 440 439 - 432 431 - 424 423 - 416

octet 48 49 50 51 52 53 54 55
bit offset 415 - 408 407 - 400 399 - 392 391 - 384 383 - 376 375 - 368 367 - 360 359 - 352

octet 56 57 58 59 60 61 62 63
bit offset 351 - 344 343 - 336 335 - 328 327 - 320 319 - 312 311 - 304 303 - 296 295 - 288

octet 64 65 66 67 68 69 70 71
bit offset 287 - 280 279 - 272 271 - 264 263 - 256 255 - 248 247 - 240 239 - 232 231 - 224

octet 72 73 74 75 76 77 78 79
bit offset 223 - 216 215 - 208 207 - 200 199 - 192 191 - 184 183 - 176 175 - 168 167 - 160

octet 80 81 82 83 84 85 86 87
bit offset 159 - 152 151 - 144 143 - 136 135 - 128 127 - 120 119 - 112 111 - 104 103 - 96

octet 88 89 90 91 92 93 94 95
bit offset 95 - 88 87 - 80 79 - 72 71 - 64 63 - 56 55 - 48 47 - 40 39 - 32

octet 96 97 98 99  
bit offset 31 - 24 23 - 16 15 - 8 7 - 0  

ErrorTypes

CodeAdditional codeNameDescription
128 (0x80)17 (0x11)Index not availableRead or write access attempt to a non-existing index.
128 (0x80)18 (0x12)Subindex not availableRead or write access attempt to a non-existing subindex of an existing index.
128 (0x80)32 (0x20)Service temporarily not availableParameter not accessible due to the current state of the technology-specific application.
128 (0x80)33 (0x21)Service temporarily unavailable - local controlParameter not accessible. The device is currently in an ongoing, locally controlled operation.
128 (0x80)34 (0x22)Service temporarily unavailable - device controlParameter not accessible. The technology-specific application is currently in a remotely triggered operation.
128 (0x80)35 (0x23)Access deniedWrite access to a read-only parameter or read access to write-only parameter.
128 (0x80)48 (0x30)Parameter value out of rangeWritten parameter value is outside of the permitted value range.
128 (0x80)49 (0x31)Parameter value above limitWritten parameter value is above its specified value range.
128 (0x80)50 (0x32)Parameter value below limitWritten parameter value is below its specified value range.
128 (0x80)51 (0x33)Parameter length overrunWritten parameter is longer than specified.
128 (0x80)52 (0x34)Parameter length underrunWritten parameter is shorter than specified.
128 (0x80)53 (0x35)Function unavailableWritten command is not supported by the technology-specific application.
128 (0x80)54 (0x36)Function temporarily unavailableWritten command is unavailable due to the current state of the technology-specific application.
128 (0x80)64 (0x40)Invalid parameter setWritten single parameter value collides with other existing parameter settings.
128 (0x80)65 (0x41)Inconsistent parameter setParameter set inconsistencies at the end of block parameter transfer. Device plausibility check failed.

Events

CodeTypeNameDescription
16912 (0x4210)WarningDevice temperature overrunClear source of heat
20753 (0x5111)WarningPrimary supply voltage underrunCheck valid voltage range
25376 (0x6320)ErrorParameter errorCheck datasheet and values
35872 (0x8c20)ErrorMeasurement range exceededCheck application
36000 (0x8ca0)WarningOutput current overloadCheck the load and current consumption.
36001 (0x8ca1)WarningOverflow Counter AbsoluteMaintenance request: The limit for switching cycles since initial commissioning has been reached. Check or replace valve and connector.
36002 (0x8ca2)WarningOverflow Counter RelativeMaintenance request: The limit for switching cycles since the last reset has been reached. Check or replace valve and connector.
36003 (0x8ca3)WarningOutput open-circuitCheck the load and valve connection.

Process Data Formatting

Formatting for Process Data id=PI_PDin
Subindex 1:
Subindex 2: * 1 + 0 % Dec.0

Formatting for Process Data id=PO_PDout
Subindex 1:
Subindex 2: * 1 + 0 % Dec.0

Operator Menus

Identification Menu
Device Information
V_VendorName
V_VendorText
V_ProductName
V_ProductText
V_ProductID
V_SerialNumber
V_XPFS_ProductURI
Revision Information
V_HardwareRevision
V_FirmwareRevision
Application Specific Information
V_ApplicationSpecificTag, ro
V_CP_FunctionTag, ro
V_CP_LocationTag, ro

Parameters Menu
Operating Parameter
V_XPFA_VMA_ConfigPWM * 1 + 0 %, ro Dec.0
V_XPFA_VMA_ConfigPickupTime * 1 + 0 ms, ro Dec.0
V_XPFA_VMA_ConfigCurrentLimit * 1 + 0 mA, ro Dec.0
V_XPFA_VMA_ConfigTempLimit * 1 + 0 °C, ro Dec.0
V_XPFA_VMA_ConfigFailSafe, ro
V_XPFA_VMA_Mode, ro
If V_XPFA_VMA_Mode = 2:
Timing Parameter (not applicable for Smart and standard mode)
V_XPFA_VMA_TimerOn * 1 + 0 s, ro Dec.0
V_XPFA_VMA_TimerOff * 1 + 0 s, ro Dec.0
If V_XPFA_VMA_Mode = 3:
Timing Parameter (not applicable for Smart and standard mode)
V_XPFA_VMA_TimerOn * 1 + 0 s, ro Dec.0
V_XPFA_VMA_TimerOff * 1 + 0 s, ro Dec.0
If V_XPFA_VMA_Mode = 4:
Timing Parameter (not applicable for Smart and standard mode)
V_XPFA_VMA_TimerOn * 1 + 0 s, ro Dec.0
V_XPFA_VMA_TimerOff * 1 + 0 s, ro Dec.0
If V_XPFA_VMA_Mode = 5:
Timing Parameter (not applicable for Smart and standard mode)
V_XPFA_VMA_TimerOn * 1 + 0 s, ro Dec.0
V_XPFA_VMA_TimerOff * 1 + 0 s, ro Dec.0
Maintenance Configuration
V_XPFA_VMA_ConfigCounterAbs, ro
V_XPFA_VMA_ConfigCounterRel, ro
Event Configuration
V_XPFA_VMA_ConfigEvent, ro
If V_XPFA_VMA_IndicationMode = 0:
Userinterface Configuration
V_XPFA_VMA_IndicationMode, ro
V_XPFA_VMA_LedColorOn, ro
V_XPFA_VMA_LedColorOff, ro
V_XPFA_VMA_LedColorWarn, ro
V_XPFA_VMA_LedModeWarn, ro
V_XPFA_VMA_Locator
If V_XPFA_VMA_IndicationMode = 1:
Userinterface Configuration
V_XPFA_VMA_IndicationMode, ro
V_XPFA_VMA_Locator

Observation Menu
Demo Menu
V_VendorName
V_ApplicationSpecificTag, ro
V_XPFA_VMA_ConfigPWM * 1 + 0 %, ro Dec.0
V_XPFA_VMA_Locator, ro
V_XPFA_VMA_MonCounterRel, ro
V_XPFA_VMA_ConfigCounterRel, ro
Measurement
V_XPFA_VMA_MonSupplyVoltage * 1 + 0 V, Dec.0
V_XPFA_VMA_MonValveCurrent * 1 + 0 mA, Dec.0
V_XPFA_VMA_MonValvePower * 1 + 0 mW, Dec.0
V_XPFA_VMA_MonTempCur * 1 + 0 °C, Dec.0
V_XPFA_VMA_MonOnResistance * 1 + 0 Ω, Dec.0
V_XPFA_VMA_MonSwitchingTime * 1 + 0 ms, Dec.0
Alarm
V_XPFA_VMA_DiagStatus.Switching Cycles Relative Overflow
V_XPFA_VMA_DiagStatus.Valve Switching Alarm
V_XPFA_VMA_DiagStatus.Open Circuit Fault

Diagnosis Menu
Device Status Information
V_DeviceStatus
V_DetailedDeviceStatus
Operating Information
V_XPFA_VMA_MonSupplyVoltage * 1 + 0 V, Dec.0
V_XPFA_VMA_MonValveCurrent * 1 + 0 mA, Dec.0
V_XPFA_VMA_MonValvePower * 1 + 0 mW, Dec.0
V_XPFA_VMA_MonOnResistance * 1 + 0 Ω, Dec.0
V_XPFA_VMA_MonSwitchingTime * 1 + 0 ms, Dec.0
V_XPFA_VMA_MonTempCur * 1 + 0 °C, Dec.0
V_XPFS_VMA_MonTempExceedCount
V_XPFA_VMA_MonTempMax * 1 + 0 °C, Dec.0
V_XPFA_VMA_Cmd, Button:=1
Description=The stored value for maximum observed device temperature is reset to the current temperature value.
Maintenance Information
V_XPFA_VMA_MonCounterAbs
V_XPFA_VMA_MonCounterRel
V_XPFA_VMA_DiagStatus
Communication Characteristics
V_DirectParameters_1.Min Cycle Time, ro
V_DirectParameters_1.Master Cycle Time, ro
V_DirectParameters_1.IO-Link Revision ID, ro
V_DirectParameters_1.Process Data Input Length, ro
V_DirectParameters_1.Process Data Output Length, ro

Maintenance Menus

Identification Menu
Device Information
V_VendorName
V_VendorText
V_ProductName
V_ProductText
V_ProductID
V_SerialNumber
V_XPFS_ProductURI
Revision Information
V_HardwareRevision
V_FirmwareRevision
Application Specific Information
V_ApplicationSpecificTag
V_CP_FunctionTag
V_CP_LocationTag

Parameters Menu
Operating Parameter
V_XPFA_VMA_ConfigPWM * 1 + 0 %, Dec.0
V_XPFA_VMA_ConfigPickupTime * 1 + 0 ms, Dec.0
V_XPFA_VMA_ConfigCurrentLimit * 1 + 0 mA, Dec.0
V_XPFA_VMA_ConfigTempLimit * 1 + 0 °C, Dec.0
V_XPFA_VMA_ConfigFailSafe
V_XPFA_VMA_Mode
If V_XPFA_VMA_Mode = 2:
Timing Parameter (not applicable for Smart and standard mode)
V_XPFA_VMA_TimerOn * 1 + 0 s, Dec.0
V_XPFA_VMA_TimerOff * 1 + 0 s, Dec.0
If V_XPFA_VMA_Mode = 3:
Timing Parameter (not applicable for Smart and standard mode)
V_XPFA_VMA_TimerOn * 1 + 0 s, Dec.0
V_XPFA_VMA_TimerOff * 1 + 0 s, Dec.0
If V_XPFA_VMA_Mode = 4:
Timing Parameter (not applicable for Smart and standard mode)
V_XPFA_VMA_TimerOn * 1 + 0 s, Dec.0
V_XPFA_VMA_TimerOff * 1 + 0 s, Dec.0
If V_XPFA_VMA_Mode = 5:
Timing Parameter (not applicable for Smart and standard mode)
V_XPFA_VMA_TimerOn * 1 + 0 s, Dec.0
V_XPFA_VMA_TimerOff * 1 + 0 s, Dec.0
Maintenance Configuration
V_XPFA_VMA_ConfigCounterAbs
V_XPFA_VMA_ConfigCounterRel
Event Configuration
V_XPFA_VMA_ConfigEvent
If V_XPFA_VMA_IndicationMode = 0:
Userinterface Configuration
V_XPFA_VMA_IndicationMode
V_XPFA_VMA_LedColorOn
V_XPFA_VMA_LedColorOff
V_XPFA_VMA_LedColorWarn
V_XPFA_VMA_LedModeWarn
V_XPFA_VMA_Locator
If V_XPFA_VMA_IndicationMode = 1:
Userinterface Configuration
V_XPFA_VMA_IndicationMode
V_XPFA_VMA_Locator
General Settings
V_SystemCommand, Button:=129
Description=The parameter of the technology-specific application are set to default values. Identification parameter remain unchanged. An upload to the data storage of the master will be executed, if activated in the port configuration of the master.

Observation Menu
Demo Menu
V_VendorName
V_ApplicationSpecificTag
V_XPFA_VMA_ConfigPWM * 1 + 0 %, Dec.0
V_XPFA_VMA_Locator
V_XPFA_VMA_MonCounterRel
V_XPFA_VMA_ConfigCounterRel
Measurement
V_XPFA_VMA_MonSupplyVoltage * 1 + 0 V, Dec.0
V_XPFA_VMA_MonValveCurrent * 1 + 0 mA, Dec.0
V_XPFA_VMA_MonValvePower * 1 + 0 mW, Dec.0
V_XPFA_VMA_MonTempCur * 1 + 0 °C, Dec.0
V_XPFA_VMA_MonOnResistance * 1 + 0 Ω, Dec.0
V_XPFA_VMA_MonSwitchingTime * 1 + 0 ms, Dec.0
Alarm
V_XPFA_VMA_DiagStatus.Switching Cycles Relative Overflow
V_XPFA_VMA_DiagStatus.Valve Switching Alarm
V_XPFA_VMA_DiagStatus.Open Circuit Fault

Diagnosis Menu
Device Status Information
V_DeviceStatus
V_DetailedDeviceStatus
Operating Information
V_XPFA_VMA_MonSupplyVoltage * 1 + 0 V, Dec.0
V_XPFA_VMA_MonValveCurrent * 1 + 0 mA, Dec.0
V_XPFA_VMA_MonValvePower * 1 + 0 mW, Dec.0
V_XPFA_VMA_MonOnResistance * 1 + 0 Ω, Dec.0
V_XPFA_VMA_MonSwitchingTime * 1 + 0 ms, Dec.0
V_XPFA_VMA_MonTempCur * 1 + 0 °C, Dec.0
V_XPFS_VMA_MonTempExceedCount
V_XPFA_VMA_MonTempMax * 1 + 0 °C, Dec.0
V_XPFA_VMA_Cmd, Button:=1
Description=The stored value for maximum observed device temperature is reset to the current temperature value.
Maintenance Information
V_XPFA_VMA_MonCounterAbs
V_XPFA_VMA_MonCounterRel
V_XPFA_VMA_DiagStatus
Communication Characteristics
V_DirectParameters_1.Min Cycle Time, ro
V_DirectParameters_1.Master Cycle Time, ro
V_DirectParameters_1.IO-Link Revision ID, ro
V_DirectParameters_1.Process Data Input Length, ro
V_DirectParameters_1.Process Data Output Length, ro
Service Functions
V_SystemCommand, Button:=130
Description=The parameter of the device are reset to factory settings. Note: A download of the data storage may be executed on the next power cycle and overwrite the factory default settings!

Commissioning Menus

Identification Menu
Device Information
V_VendorName
V_VendorText
V_ProductName
V_ProductText
V_ProductID
V_SerialNumber
V_XPFS_ProductURI
Revision Information
V_HardwareRevision
V_FirmwareRevision
Application Specific Information
V_ApplicationSpecificTag
V_CP_FunctionTag
V_CP_LocationTag

Parameters Menu
Operating Parameter
V_XPFA_VMA_ConfigPWM * 1 + 0 %, Dec.0
V_XPFA_VMA_ConfigPickupTime * 1 + 0 ms, Dec.0
V_XPFA_VMA_ConfigCurrentLimit * 1 + 0 mA, Dec.0
V_XPFA_VMA_ConfigTempLimit * 1 + 0 °C, Dec.0
V_XPFA_VMA_ConfigFailSafe
V_XPFA_VMA_Mode
If V_XPFA_VMA_Mode = 2:
Timing Parameter (not applicable for Smart and standard mode)
V_XPFA_VMA_TimerOn * 1 + 0 s, Dec.0
V_XPFA_VMA_TimerOff * 1 + 0 s, Dec.0
If V_XPFA_VMA_Mode = 3:
Timing Parameter (not applicable for Smart and standard mode)
V_XPFA_VMA_TimerOn * 1 + 0 s, Dec.0
V_XPFA_VMA_TimerOff * 1 + 0 s, Dec.0
If V_XPFA_VMA_Mode = 4:
Timing Parameter (not applicable for Smart and standard mode)
V_XPFA_VMA_TimerOn * 1 + 0 s, Dec.0
V_XPFA_VMA_TimerOff * 1 + 0 s, Dec.0
If V_XPFA_VMA_Mode = 5:
Timing Parameter (not applicable for Smart and standard mode)
V_XPFA_VMA_TimerOn * 1 + 0 s, Dec.0
V_XPFA_VMA_TimerOff * 1 + 0 s, Dec.0
Maintenance Configuration
V_XPFA_VMA_ConfigCounterAbs
V_XPFA_VMA_ConfigCounterRel
Event Configuration
V_XPFA_VMA_ConfigEvent
If V_XPFA_VMA_IndicationMode = 0:
Userinterface Configuration
V_XPFA_VMA_IndicationMode
V_XPFA_VMA_LedColorOn
V_XPFA_VMA_LedColorOff
V_XPFA_VMA_LedColorWarn
V_XPFA_VMA_LedModeWarn
V_XPFA_VMA_Locator
If V_XPFA_VMA_IndicationMode = 1:
Userinterface Configuration
V_XPFA_VMA_IndicationMode
V_XPFA_VMA_Locator
General Settings
V_SystemCommand, Button:=129
Description=The parameter of the technology-specific application are set to default values. Identification parameter remain unchanged. An upload to the data storage of the master will be executed, if activated in the port configuration of the master.

Observation Menu
Demo Menu
V_VendorName
V_ApplicationSpecificTag
V_XPFA_VMA_ConfigPWM * 1 + 0 %, Dec.0
V_XPFA_VMA_Locator
V_XPFA_VMA_MonCounterRel
V_XPFA_VMA_ConfigCounterRel
Measurement
V_XPFA_VMA_MonSupplyVoltage * 1 + 0 V, Dec.0
V_XPFA_VMA_MonValveCurrent * 1 + 0 mA, Dec.0
V_XPFA_VMA_MonValvePower * 1 + 0 mW, Dec.0
V_XPFA_VMA_MonTempCur * 1 + 0 °C, Dec.0
V_XPFA_VMA_MonOnResistance * 1 + 0 Ω, Dec.0
V_XPFA_VMA_MonSwitchingTime * 1 + 0 ms, Dec.0
Alarm
V_XPFA_VMA_DiagStatus.Switching Cycles Relative Overflow
V_XPFA_VMA_DiagStatus.Valve Switching Alarm
V_XPFA_VMA_DiagStatus.Open Circuit Fault

Diagnosis Menu
Device Status Information
V_DeviceStatus
V_DetailedDeviceStatus
Operating Information
V_XPFA_VMA_MonSupplyVoltage * 1 + 0 V, Dec.0
V_XPFA_VMA_MonValveCurrent * 1 + 0 mA, Dec.0
V_XPFA_VMA_MonValvePower * 1 + 0 mW, Dec.0
V_XPFA_VMA_MonOnResistance * 1 + 0 Ω, Dec.0
V_XPFA_VMA_MonSwitchingTime * 1 + 0 ms, Dec.0
V_XPFA_VMA_MonTempCur * 1 + 0 °C, Dec.0
V_XPFS_VMA_MonTempExceedCount
V_XPFA_VMA_MonTempMax * 1 + 0 °C, Dec.0
V_XPFA_VMA_Cmd, Button:=1
Description=The stored value for maximum observed device temperature is reset to the current temperature value.
Maintenance Information
V_XPFA_VMA_MonCounterAbs
V_XPFA_VMA_MonCounterRel
V_XPFA_VMA_DiagStatus
Communication Characteristics
V_DirectParameters_1.Min Cycle Time, ro
V_DirectParameters_1.Master Cycle Time, ro
V_DirectParameters_1.IO-Link Revision ID, ro
V_DirectParameters_1.Process Data Input Length, ro
V_DirectParameters_1.Process Data Output Length, ro
Service Functions
V_SystemCommand, Button:=130
Description=The parameter of the device are reset to factory settings. Note: A download of the data storage may be executed on the next power cycle and overwrite the factory default settings!

Note: This page shows the content of an IODD file transformed into HTML format. In the case of disparity between this and the XML view, the content of the XML file takes precedence.
Created by IODD Viewer V1.4.